SLAZ753C October 2025 – November 2025 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1
ADC Module
Functional
HW Event generated before enabling IP, ADC Trigger will stay in queue
When the ADC receives a HW event trigger the pending event will go into the ADC trigger queue, even if CTL0.ENC = 0x0. Once ADC is set to CTL1.TRIGSRC = 0x1 (HW Trigger) and CTL0.ENC = 1 then the queued HW trigger will start the ADC sampling and conversion process. The pending HW request can get into the queue even when the CTL1.TRIGSRC = 0x0 (SW trigger), but will only start the ADC sampling when CTL1.TRIGSRC = 0x1 && CTL0.ENC = 0x1.
Only configure the ADC F_SUB when expecting to use the HW Trigger, otherwise a pending request can get queued. If switching between SW and HW Trigger modes, a reset on the ADC (RSTCTL) will clear any pending queues, but will require the ADC to be reconfigured.