SLAZ753C October 2025 – November 2025 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1
UART Module
Functional
UART Receive timeout starts counting earlier than expected during the STOP bit transaction
During the STOP bit transaction the Receive timeout will start counting in the middle of the STOP bit transaction, which can cause an unintended RTOUT interrupt if the RXTOSEL setting is too small. For example, if the baud rate was 1Mbps, and RXTOSEL was set to 1, the expected RTOUT should happen 1us after the STOP bit transaction, instead the RTOUT interrupt is getting set at 0.5 us.
The UART.IFLS.RXTOSEL register selects the bit time before the Receive Time out (RTOUT) interrupt will fire. The RXTOSEL value needs to be greater than 1 in order to prevent an early interrupt. The receive timeout time can be calculated as: Receive timeout = (RXTOSEL - 0.5) / Baud Rate