SLAZ753C October 2025 – November 2025 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1
CPU Module
Functional
Prefetcher can fetch wrong instructions when transitioning into Low power modes
When transitioning into low power modes and there is a pending prefetch, the prefetcher can erroneously fetch incorrect data (all 0's). When the device wakes up, if the prefetcher and cache do not get overwritten by ISR code, then the main code execution from flash can get corrupted. For example, if the ISR is in the SRAM, then the incorrect data that was prefetched from Flash does not get overwritten. When the ISR returns the corrupted data in the prefetcher can be fetched by the CPU resulting in incorrect instructions. A HW Event wake is another example of a process that will wake the device, but not flush the prefetcher.
Disable prefetcher before entering low power modes.
Example:
CPUSS.CTL.PREFETCH = 0x0; // disables prefetcher
SYSCTL.SOCLOCK.SHUTDNSTORE0 // Read from SHUTDOWN Memory
__WFI(); // or __WFE(); this function calls the transition into low power mode
CPUSS.CTL.PREFETCH = 0x1; // enables prefetcher