SLCA006A June 2025 – July 2026 LM339 , LM393 , LMH7322 , TL331 , TLV1812 , TLV1871 , TLV1872 , TLV3211 , TLV3211-Q1 , TLV3601 , TLV3604
The Open Collector or Open Drain (used interchangeably) output consists of a single transistor that can only sink current. This can be thought as a mechanical (SPST) switch from the output to ground.
A pull-up resistor is required to create the output high voltage. The termination voltage applied to the top of the termination resistor sets the output high (VOH) voltage. When the output is logic High, the transistor is off (not conducting), and the pull-up resistor pulls the output node up to the termination voltage.
NOTE: The output can be pulled up to any voltage less than the comparator supply voltage. In most cases, the comparator allows the output to be pulled above the comparator supply voltage up to a maximum voltage. However, some devices have an upper ESD clamp diode on the output that limits the maximum pull-up voltage to the supply voltage. Pulling up to a different voltage is known as Level-Shifting.
The data sheet Features or Electrical Specification table notes can mention if the output can be pulled above the supply. If not, then the Output Voltage line of the Absolute Maximum Ratings or Recommended Operating Conditions can give a clue.
An advantage of the open collector output is that multiple outputs can be tied together to form a OR'ed output bus, where any output can pull the output bus low. This is common for system error buses and window comparators.
A list of Open Collector output devices is shown in Table 3-1.
| Advantages | Disadvantages |
|---|---|
|
|