SLLA682 July 2025 TDP142
The entirety of any high-speed signal trace needs to maintain the same GND reference plane from origination to termination. If the same GND reference plane is not maintained, via-stitch both GND planes together to make sure continuous grounding and uniform impedance. Place these stitching vias symmetrically within 200mils (Center-to-center, closer is better) of the signal transition vias. See Figure 6-3 for an example of GND stitching vias.
Figure 6-3 GND Stitching Vias
Example