The following layout guidelines needs to be used
in routing the high-speed DisplayPort signals to and from the TDP142.
- INDP and OUTDP pairs must be routed
with controlled 100Ω differential impedance (±10%).
- Keep differential pairs away from
other high-speed signals.
- Intra-pair routing needs to be kept
to within 5 mils.
- DisplayPort lane inter-pair routing
needs to be kept to within 2 UI according to the DisplayPort Design Guide.
- Differential pair length matching
needs to be near the location of mismatch.
- Each pair needs to be separated by
at least 3 times the signal trace width.
- The use of bends in differential
traces needs to be kept to a minimum. When bends are used, the number of left
and right bends needs to be as equal as possible and the angle of the bend needs
to be ≥ 135°. This can minimize any length mismatch caused by the bends and
minimize the impact bends have on EMI.
- Route all differential pairs on the
same layer.
- Minimize the number of vias, this
is recommended to keep the via count to 2 or less.
- The layout can face signal
crossing on OUTDP2 and OUTDP3 due to mismatched order between the output pins of
the device and the connector. One of the designs is to do polarity swap on the
input of the device when GPU is BGA package. This can minimize the number of
VIAS being used. Please refer to Figure 6-1 and Figure 6-2.
- Keep differential traces on layers adjacent to a ground plane.
- Do not route differential pairs
over any split plane.
- If using a through-hole connector,
route the high-speed signals on opposite side of the connector such that the
connector pin does not create a stub in the transmission line.
- Test points needs to be placed in
series and in symmetry to avoid impedance discontinuity.