SLLA682 July 2025 TDP142
This section discusses an example to select equalization for different trace length. Figure 4-1 shows an example sink side application of TDP142. The following method is used to select equalization value for this sink side application:
Other factors such as layout quality and DP driver and receiver quality can require the equalization settings to be adjusted higher or lower for best performance. The previous method is recommended to be used for selecting initial configuration settings based on system board trace lengths.