SLLSEY7G June 2017 – February 2025 ISO1211 , ISO1212
PRODUCTION DATA
The ISO121x devices provide an output-enable pin on the controller side (EN). Setting the EN pin to 0 causes the output buffers to be in the high-impedance state. This feature can be used to multiplex the outputs of multiple ISO121x devices on the same host-controller input, reducing the number of pins on the host controller.
In the example shown in Figure 8-11, two sets of 8-channel inputs are multiplexed, reducing the number of input pins required on the controller from 16 to 10. Similarly, if four sets of 8-channel inputs are multiplexed, the number of pins on the controller is reduced from 32 to 12.
Figure 8-11 Using the Output Enable Option to Multiplex the Interface to the Host Controller