SLLSFO6A May 2024 – December 2025 TCAN2410-Q1 , TCAN2411-Q1
PRODUCTION DATA
The normal sequence summary is as follows:
See Table 8-22 for an example of the first loop sequence.
| Step | Register | Data | Description |
|---|---|---|---|
| 1 | WD_QA_QUESTION (0x2F) | [R] 0x0C | Read the question. Question is 0x0C |
| 2 | WD_QA_ANSWER (0x2E) | [W] 0x58 | Write answer 3 (See Table 8-18 Example answers to questions with default settings to see answers) |
| 3 | WD_QA_ANSWER (0x2E) | [W] 0xA8 | Write answer 2 |
| 4 | WD_QA_ANSWER (0x2E) | [W] 0x57 | Write answer 1 |
| 5 | WD_QA_ANSWER (0x2E) | [W] 0xA7 | Write answer 0 once window 2 has started |
At this point, the user can read the WD_QA_QUESTION[6] (0x2F) register to determine if WD_QA_ERR is set.