SLLU383A October   2024  – July 2025

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Device Information
    4. 1.4 Specification
  8. 2Hardware
    1. 2.1 Quick Start Guide
    2. 2.2 Hardware Setup
    3. 2.3 Hardware Connections Overview
    4. 2.4 Connection Details
    5. 2.5 MSP430FR2355 Microcontroller
    6. 2.6 LED Lights
    7. 2.7 User Configurable Settings
  9. 3Software
    1. 3.1 Firmware and GUI Application
    2. 3.2 Downloading and Running Motor Studio
    3. 3.3 Downloading Code Composer Studio and Importing GUI Firmware
    4. 3.4 Using eZ-FET to Program the Onboard MSP430FR2355
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layouts
    3. 4.3 Bill of Materials (BOM)
  11. 5Additional Information
    1. 5.1 Trademarks
  12. 6Revision History

Quick Start Guide

The MCF8329RRYEVM requires a power supply source, which has a recommended operating range from a 4.5V to 60V. To setup and power the EVM, follow the sequence below:

  1. Connect motor phases to A, B, and C on connector J11.
  2. Do not turn on the power supply yet. Connect the motor supply to PVDD and GND on connector J10.
  3. Select J6 to 5V_USB and J8 to 3V3COM to power MSP430 from USB power supply.
  4. Connect the micro-USB cable into the computer.
  5. Turn the potentiometer fully clockwise to set the motor to zero speed upon power up.
  6. Flip Switch S2 to the top to set DRVOFF on, S3 to the bottom to set DIR as ABC, and S4 to the bottom to set the set the device to the WAKE state.
  7. Flip switch S1 into the down position to set the EVM to support the MCF8329A-Q1.
  8. Set the jumper on J13 to the POT position to apply the analog voltage from potentiometer R47 to the SPEED/WAKE pin.
  9. Turn on the motor power supply.
  10. Use the potentiometer R47 to control the speed of the motor and the switches to disable the motor driver, change the direction, or apply a brake to the motor. Optionally, use the GUI to monitor the real-time speed of the motor, put the MCF8329 into a low-power sleep mode, and read status of the LEDs as shown in Section 3.
Note: If using the MCF8329B-Q1, then set S1 into the up position to set the EVM to support the MCF8329B-Q1.
MCF8329RRYEVM Reference for Quick Start
                    Guide Figure 2-1 Reference for Quick Start Guide