SLOU590 January 2025 TAS5802 , TAS5815
The high-level path, similar to the low-level path, has 1 Biquad that can set the EQ curve used when the time averaged input signal is above the upper mixing threshold.