SLOU590 January 2025 TAS5802 , TAS5815
Figure 3-6 shows the default volume in PPC3 GUI. Note that volume needs to be specified in decibels (dB). Independent volume change for left and right channel can be achieved by deselecting the “Gang” option.
Figure 3-6 VolumeThe volume block is implemented using an alpha filter structure. As Figure 3-7 shows, when a volume level change is initiated, the volume block provides a smooth transition to the newly commanded volume level without producing artifacts such as pops and clicks.
Figure 3-7 Volume Attack and Release