SLUSEE5E January 2022 – April 2026 TPS4811-Q1
PRODUCTION DATA
When the external MOSFETs turn OFF during the conditions such as INP control, overvoltage cutoff, overcurrent protection causing an interruption of the current flow, the input parasitic line inductance generates a positive voltage spike on the input and output parasitic inductance generates a negative voltage spike on the output. The peak amplitude of voltage spikes (transients) depends on the value of inductance in series to the input or output of the device. These transients can exceed the Absolute Maximum Ratings of the device if steps are not taken to address the issue. Typical methods for addressing transients include:
The TPS4811Q1 gets powered from the VS pin. Voltage at this pin must be maintained above V(VS_PORR) level to ensure proper operation. If the input power supply source is noisy with transients, then TI recommends to place a RVS - CVS filter between the input supply line and VS pin to filter out the supply noise. TI recommends RVS value around 100Ω.
In case where large di/dt is involved, the system and layout parasitic inductances can generate large differential signal voltages between ISCP and CS- pins. This action can trigger false short-circuit protection and nuisance trips in the system. To overcome such scenario, TI recommends to add filter capacitor of 1nF (CSCP) across ISCP and CS- pins close to the device. Because nuisance trips are dependent on the system and layout parasitics, TI recommends to test the design in a real system and tweaked as necessary.
The following figure shows the circuit implementation with optional protection components.
| Component Designator | Description | Recommended Value |
|---|---|---|
| RVS, CVS | TPS4811Q1 gets powered from the VS pin. Voltage at this pin must be maintained above V(VS_PORR) level to ensure proper operation during noisy line transients. | 100Ω, 0.1-10µF |
| CISCP | In a case where large di/dt is involved, the system and layout parasitic inductances can generate large differential signal voltages between CS1+ and CS1– pins. This action can trigger false short-circuit protection and nuisance trips in the system. To overcome such scenario, TI suggests to add a placeholder for RC filter components across the sense resistor (RSNS) and tweak the values during test in the real system. Capacitor (CISCP) across ISCP and DRN pins can also be placed to avoid false short-circuit protection (SCP) during inrush duration or startup. | 0.001-1µF |
| FB1, FB2, CCS, CCS1+, CCS1-, CIMON, CIWRN | Ferrite beads (FB1, FB2 ) can be required at CS1+ and CS1- pins for better immunity performance during EMI/EMC testing. Ferrite beads must be selected such that DC Resistance is very low on CS- pin to avoid significantly impacting IMON accuracy. Some other filtering can also be required based on type of immunity test and frequency band through CCS, CCS1+, CCS1-, CIMON, CIWRN to achieve robust immunity performance. | MMZ1608B102CTA00, 10pF for CTMP, CIOC and 10pF - 100nF for others |
| RGATE_PU, RGATE_PD, D3 | Resistors on GATE pins can be used for controlling rise and fall time of external FETs. Separate RGATE_PU must be used for individual external FETs connected in parallel. | Any value |
| CEN | If EN is derived from input supply then CEN can be used to filter supply line transients and avoid false UVLO trigger. | 1 - 1000nF |
| RINP, RFLT_I, RFLT_T | INP, FLT_I, FLT_T, pins needs to be connected to MCU or other HI/LO source through a resistor for protection especially for reverse polarity fault events. | 1 - 10kΩ |
| CFLT_I, CFLT_T | Capacitor on FLT_I, FLT_T pins can be used for masking faults | Any value |