SLUU885C March 2012 – June 2024 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138A , UCD3138A64
After click the tab of Designer, the page is shown as in Figure 14-3. In the UCD3138PFCEVM-026, this page is dedicated to the feedback loop design. This page including two sub-pages. One is for the current loop PID coefficients and the other is for the voltage feedback loop which uses PI control.
Figure 14-3 Page of Designer