SLUU885C March   2012  – June 2024 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138A , UCD3138A64

 

  1.   1
  2.   2
  3.   Abstract
  4. 1 Introduction
  5. 2 Description
    1. 2.1 Typical Applications
    2. 2.2 Features
  6. 3 Electrical Performance Specifications
  7. 4 Schematics
  8. 5 Test Setup
    1. 5.1 Test Equipment
    2. 5.2 Recommended Test Setup
  9. 6 List of Test Points
  10. 7 List of Terminals
  11. 8 Test Procedure
    1. 8.1 Efficiency Measurement Procedure
    2. 8.2 Equipment Shutdown
  12. 9 Performance Data and Typical Characteristic Curves
    1. 9.1 Efficiency
    2. 9.2 Power Factor
    3. 9.3 Total Harmonic Distortion (THD)
    4. 9.4 Input Current at 230 VAC and 50 Hz
    5. 9.5 Output Voltage Ripple
    6. 9.6 Output Turn On
    7. 9.7 Total Harmonic Distortion (THD)
    8. 9.8 Other Waveforms
  13. 10EVM Assembly Drawing and PCB Layout
  14. 11List of Materials
  15. 12Digital PFC Description
    1. 12.1  1PFC Block Diagram
      1. 12.1.1 Single-Phase PFC Block Diagram
      2. 12.1.2 2-Phase PFC Block Diagram
      3. 12.1.3 Bridgeless PFC Block Diagram
    2. 12.2  UCD3138 Pin Definition
      1. 12.2.1 UCD3138 Pin Definition in Single-Phase PFC
      2. 12.2.2 UCD3138 Pin Definition in 2-Phase PFC
      3. 12.2.3 UCD3138 Pin Definition in Bridgeless PFC
    3. 12.3  EVM Hardware – Introduction
      1. 12.3.1 PFC Pre-Regulator Input
      2. 12.3.2 PFC Power Stage
      3. 12.3.3 Non-Isolated UART Interface
      4. 12.3.4 Isolated UART Interface
      5. 12.3.5 Interface Connector of Control Card
      6. 12.3.6 UCD3138 Resource Allocation for PFC Control
    4. 12.4  EVM Firmware – Introduction
      1. 12.4.1 Background Loop
      2. 12.4.2 Voltage Loop Configuration
      3. 12.4.3 Current Loop Configuration
      4. 12.4.4 Interrupts
    5. 12.5  State Machine
    6. 12.6  PFC Control Firmware
    7. 12.7  System Protection
      1. 12.7.1 Cycle-by-Cycle Current Protection (CBC)
      2. 12.7.2 Over-Voltage Protection (OVP)
    8. 12.8  PFC System Control
      1. 12.8.1 Average Current Mode Control
      2. 12.8.2 ZVS and Valley Control
    9. 12.9  Current Feedback Control Compensation Using PID Control
      1. 12.9.1 Loop Compensation from Poles and Zeros in s-Domain
      2. 12.9.2 Feedback Loop Compenstaion Tuning with PID Coefficients
      3. 12.9.3 Feedback Loop Compensation with Multiple-Set of Parameters
    10. 12.10 Voltage Feedback Loop
  16. 13Evaluating the Single-Phase PFC with GUI
    1. 13.1 Graphical User Interface (GUI)
    2. 13.2 Open the Designer GUI
    3. 13.3 Overview of the Designer GUI
      1. 13.3.1 Monitor
      2. 13.3.2 Status
      3. 13.3.3 Design and Configure
  17. 14Monitoring, Re-configuring and Re-tuning with Designer GUI
    1. 14.1 Power On and Test Procedure
    2. 14.2 Monitoring with GUI
    3. 14.3 Configuration and Re-configuring with GUI
    4. 14.4 Feedback Control Loop Tuning and Re-Tuning with GUI
      1. 14.4.1 Current Loop Evaluation
      2. 14.4.2 Current Loop Re-Tuning
      3. 14.4.3 Voltage Loop Evaluation and Re-tuning
  18. 15Digital PFC Firmware Development
  19. 16References
  20. 17Revision History

Current Loop Re-Tuning

The current loop PID coefficients can be re-tuned following the approaches described in section 1.4. Scroll down the window that is shown in Figure 12-13, then Figure 14-5 is obtained.

Figure 12-13 shows the current loop compensation details. There are two sets of PID coefficients used in the current control loop, Set A and Set B. In Figure 14-5 Set A is shown. The corresponding bode plots are shown on the left in Figure 14-5.

Coefficients of Set A are used when input line voltage is between 90 VAC and 160 VAC. Coefficients of Set B are used when input line voltage is above 160 VAC till the maximum input of 264 VAC.

The actual PID control makes re-scale of the values shown in Figure 14-5 when used inside the UCD3138.

Equation 18.

PRD is a threshold value used to generate DPWM cycle ending point. The DPWM is centered on a period counter which counts up from 0 to PRD, and then is reset and starts over again. In the single-phase PFC design, KCOMP is set up equal to PRD.

In the current control page of the Design, PID coefficients can be re-tuned. The GUI also provides conversion results from PID coefficients to the zeros and the pole by clicking Mode to select a corresponding conversion. One can also change the zeros and the poles and then use the GUI to convert to PID coefficients by clicking Mode to select back to KP, KI, and KD. Be aware that from the two zeros can be complex conjugates. When a set of PID coefficients does make complex conjugate zeros, the GUI pumps up a message to notify that Q and ωr have to be generated instead of real zeros. In this case, the users may need to calculate the complex conjugate zeros based on Equation 6.

 Current Loop Re-TuningFigure 14-5 Current Loop Re-Tuning