The upper section of the Firmware screen is used to initialize the device by loading the default .srec into the flash memory (see Figure 2-6).
- Search for the .srec file using the Browse button.
- Select the Execute after programming box to automatically return the device to Normal mode after programming has completed.
- Press the Program button and wait for the download to complete.