SLUUDG7 December 2025 MSPM33C321A , MSPM33C321A-Q1
The security attribution unit (SAU) can be used by the programmer to define regions of memories security. The final security level uses both the SAU configuration and the IDAU configuration. For determining a section of memories security level take the higher security level between the SAU and IDAU. For example if the SAU defines a region as secure and the IDAU defines a region as non-secure the region is defined as secure.
On the MSPM33 devices the SAU is built to support defining 8 regions as Secure, non-secure, or non-secure callable.
One major use case for the SAU is for is defining a region as secure or non-secure. To define a region the following steps are taken by writing to the SAU's registers