SLUUDJ2 May   2026

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  6. 2Hardware
    1. 2.1 General Usage Information
  7. 3Implementation Results
    1. 3.1 Test Setup Diagrams
      1. 3.1.1 S-Parameter Test Setup
      2. 3.1.2 Noise Figure Test Setup
      3. 3.1.3 Two-Tone OIP3 Test Setup
  8. 4Hardware Design Files
    1. 4.1 Schematic
    2. 4.2 PCB Layers
      1. 4.2.1 Stack-Up and Material
    3. 4.3 TRF0108SP/SEP-EVM Bill of Material
  9. 5Additional Information
    1. 5.1 Trademarks
  10. 6Related Documentation

Noise Figure Test Setup

TRF0108SP-EVM TRF0108SEP-EVM Noise Figure Test
                    Setup Figure 3-3 Noise Figure Test Setup

Use the following guidelines for noise figure (NF) measurement:

  1. As shown in Figure 3-3, the traditional Y-factor method can be used for the NF measurement using a noise diode and a spectrum analyzer (or a noise figure analyzer).
  2. For accurate NF measurement, account for RF cable losses to the EVM and for any external attenuators used in the setup
  3. Also, onboard losses of the input traces at the device input pins must be factored into the NF measurement
  4. If the loss after the device output is significant (greater than about 5dB) then factor the output loss into the NF measurement. Use the Friis equation to calculate the NF of the device from the total measured NF.