SLVAES8A May   2020  – February 2026 DRV8424 , DRV8424E , DRV8426 , DRV8428 , DRV8428E , DRV8434 , DRV8434E , DRV8434S , DRV8436 , DRV8436E , DRV8889-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Details of the Test Setup
  6. 3Sources of Noise in a Stepper Motor
    1. 3.1 Magnetic Noise
    2. 3.2 Mechanical Noise
    3. 3.3 Electrical Noise
      1. 3.3.1 Effects of Current Ripple and Decay Mode
      2. 3.3.2 Effects of PWM Chopper Frequency
      3. 3.3.3 Effects of Current Zero-Cross Error
      4. 3.3.4 Effects of Step Resolution and Step Frequency
      5. 3.3.5 Effects of Resonant Frequency
  7. 4Summary
  8. 5References
  9. 6Revision History

Effects of PWM Chopper Frequency

If the PWM frequency falls within the audible band, it manifests itself as a whine coming out of the stepper motor. Even when the motor is stopped and holds the position, the noise associated with PWM frequency will be audible. If the chopping frequency is ultrasonic, a hissing sound can be heard.

Legacy stepper drivers often have a pin which controls the OFF time of the PWM by using two R-C passive components. Designs with 50µs OFF time are common. When the ON time is added to the OFF time, the resulting PWM frequency are less than 20kHz and generate audible noise. Therefore, it can be concluded that noise can be reduced by increasing the PWM frequency. Too high PWM frequency also leads to higher switching losses, therefore it may not be desirable to increase the frequency well above the audible range. An appropriate PWM frequency value will be between 30kHz and 50kHz.

Equation 1 shows the approximate relation between the PWM frequency and the current ripple for the smart tune Ripple Control decay mode. VM is the supply voltage, VBEMF is the back-emf voltage, L is the inductance of the motor coil and ΔI is the ripple current. As is evident, PWM frequency will be high when the ripple current is low.

Equation 1.

Figure 3-12 to Figure 3-15 show the PWM frequencies at different current levels for DRV8424 smart tune Ripple Control and 1/4 microstepping. The PWM frequencies range between 25kHz and 55kHz, well beyond the audible range. In general, lowest current ripple results in PWM frequencies that fall beyond 20kHz and therefore do not impact the audible noise levels from the stepper motor.

 PWM at 38% Level, PWM
                        Frequency is 55kHzFigure 3-12 PWM at 38% Level, PWM Frequency is 55kHz
 PWM at 100% Level, PWM
                        Frequency is 35kHzFigure 3-14 PWM at 100% Level, PWM Frequency is 35kHz
 PWM at 92% Level
                        (increasing), PWM Frequency is 44kHzFigure 3-13 PWM at 92% Level (increasing), PWM Frequency is 44kHz
 PWM at 92% Level
                        (decreasing), PWM Frequency is 25kHzFigure 3-15 PWM at 92% Level (decreasing), PWM Frequency is 25kHz