SLVAG09 September 2025 TPS1HTC100-Q1 , TPS1HTC30-Q1 , TPS2HC08-Q1 , TPS2HCS08-Q1 , TPS482H85-Q1
The identification tables below help reference the waveform for each test. In place of the time to charge the capacitor, in Section 4, is a number that corresponds to the relevant figure number. All of the figures in this section are labeled as 5-#. The second number is the number from the key table. For example, to look at waveform 6 from the Table 5-1, please refer to Figure 5-6.
|
TPS1HTC30-Q1 |
Capacitor Charging Time (VS = 48V) |
|||||
|---|---|---|---|---|---|---|
|
25°C |
85°C |
|||||
|
CL Lower Limit |
CL Midpoint |
CL Upper Limit |
CL Lower Limit |
CL Midpoint |
CL Upper Limit |
|
|
Capacitance (uF) |
RCL=50kΩ, ICL=2A, RL=48Ω, IL=1A |
RCL=20kΩ, ICL=5A, RL=19.2Ω, IL=2.5A |
RCL=10kΩ, ICL=10A, RL=9.6Ω, IL=5A |
RCL=50kΩ, ICL=2A, RL=48Ω, IL=1A |
RCL=20kΩ, ICL=5A, RL=19.2Ω, IL=2.5A |
RCL=10kΩ, ICL=10A, RL=9.6Ω, IL=5A |
|
6.8 |
1 |
14 |
26 |
37 |
50 |
62 |
|
10 |
2 |
15 |
27 |
38 |
51 |
63 |
|
15 |
3 |
16 |
28 |
39 |
52 |
64 |
|
22 |
4 |
17 |
29 |
40 |
53 |
65 |
|
33 |
5 |
18 |
30 |
41 |
54 |
66 |
|
47 |
6 |
19 |
31 |
42 |
55 |
67 |
|
68 |
7 |
20 |
32 |
43 |
56 |
68 |
|
75 |
8 |
21 |
33 |
44 |
57 |
69 |
|
82 |
9 |
22 |
34 |
45 |
58 |
70 |
|
100 |
10 |
23 |
35 |
46 |
59 |
71 |
|
180 |
11 |
24 |
36 |
47 |
60 |
72 |
|
220 |
12 |
25 |
- |
48 |
61 |
- |
|
330 |
13 |
- |
- |
49 |
- |
- |
|
TPS1HTC100-Q1 |
Capacitor Charging Time (VS = 48V) |
|||||
|---|---|---|---|---|---|---|
|
25°C |
85°C |
|||||
|
CL Lower Limit |
CL Midpoint |
CL Upper Limit |
CL Lower Limit |
CL Midpoint |
CL Upper Limit |
|
|
Capacitance (uF) |
RCL=50kΩ, ICL=0.92A, RL=104.3Ω, IL=0.46A |
RCL=16.7kΩ, ICL=3A, RL=32Ω, IL=1.5A |
RCL=10kΩ, ICL=5.3A, RL=18.1Ω, IL=2.65A |
RCL=50kΩ, ICL=0.92A, RL=104.3Ω, IL=0.46A |
RCL=16.7kΩ, ICL=3A, RL=32Ω, IL=1.5A |
RCL=10kΩ, ICL=5.3A, RL=18.1Ω, IL=2.65A |
|
6.8 |
73 |
80 |
86 |
91 |
98 |
104 |
|
10 |
74 |
81 |
87 |
92 |
99 |
105 |
|
15 |
75 |
82 |
88 |
93 |
100 |
106 |
|
22 |
76 |
83 |
89 |
94 |
101 |
107 |
|
33 |
77 |
84 |
90 |
95 |
102 |
108 |
|
47 |
78 |
85 |
- |
96 |
103 |
- |
|
68 |
79 |
- |
- |
97 |
- |
- |
Figure 5-1 Test Condition 1
Figure 5-3 Test Condition 3
Figure 5-5 Test Condition 5
Figure 5-7 Test Condition 7
Figure 5-9 Test Condition 9
Figure 5-11 Test Condition 11
Figure 5-13 Test Condition 13
Figure 5-15 Test Condition 15
Figure 5-17 Test Condition 17
Figure 5-19 Test Condition 19
Figure 5-21 Test Condition 21
Figure 5-23 Test Condition 23
Figure 5-25 Test Condition 25
Figure 5-27 Test Condition 27
Figure 5-29 Test Condition 29
Figure 5-31 Test Condition 31
Figure 5-33 Test Condition 33
Figure 5-35 Test Condition 35
Figure 5-37 Test Condition 37
Figure 5-39 Test Condition 39
Figure 5-41 Test Condition 41
Figure 5-43 Test Condition 43
Figure 5-45 Test Condition 45
Figure 5-47 Test Condition 47
Figure 5-49 Test Condition 49
Figure 5-51 Test Condition 51
Figure 5-53 Test Condition 53
Figure 5-55 Test Condition 55
Figure 5-57 Test Condition 57
Figure 5-59 Test Condition 59
Figure 5-61 Test Condition 61
Figure 5-63 Test Condition 63
Figure 5-65 Test Condition 65
Figure 5-67 Test Condition 67
Figure 5-69 Test Condition 69
Figure 5-71 Test Condition 71
Figure 5-73 Test Condition 73
Figure 5-75 Test Condition 75
Figure 5-77 Test Condition 77
Figure 5-79 Test Condition 79
Figure 5-81 Test Condition 81
Figure 5-83 Test Condition 83
Figure 5-85 Test Condition 85
Figure 5-87 Test Condition 87
Figure 5-89 Test Condition 89
Figure 5-91 Test Condition 91
Figure 5-93 Test Condition 93
Figure 5-95 Test Condition 95
Figure 5-97 Test Condition 97
Figure 5-99 Test Condition 99
Figure 5-101 Test Condition 101
Figure 5-103 Test Condition 103
Figure 5-105 Test Condition 105
Figure 5-107 Test Condition 107
Figure 5-2 Test Condition 2
Figure 5-4 Test Condition 4
Figure 5-6 Test Condition 6
Figure 5-8 Test Condition 8
Figure 5-10 Test Condition 10
Figure 5-12 Test Condition 12
Figure 5-14 Test Condition 14
Figure 5-16 Test Condition 16
Figure 5-18 Test Condition 18
Figure 5-20 Test Condition 20
Figure 5-22 Test Condition 22
Figure 5-24 Test Condition 24
Figure 5-26 Test Condition 26
Figure 5-28 Test Condition 28
Figure 5-30 Test Condition 30
Figure 5-32 Test Condition 32
Figure 5-34 Test Condition 34
Figure 5-36 Test Condition 36
Figure 5-38 Test Condition 38
Figure 5-40 Test Condition 40
Figure 5-42 Test Condition 42
Figure 5-44 Test Condition 44
Figure 5-46 Test Condition 46
Figure 5-48 Test Condition 48
Figure 5-50 Test Condition 50
Figure 5-52 Test Condition 52
Figure 5-54 Test Condition 54
Figure 5-56 Test Condition 56
Figure 5-58 Test Condition 58
Figure 5-60 Test Condition 60
Figure 5-62 Test Condition 62
Figure 5-64 Test Condition 64
Figure 5-66 Test Condition 66
Figure 5-68 Test Condition 68
Figure 5-70 Test Condition 70
Figure 5-72 Test Condition 72
Figure 5-74 Test Condition 74
Figure 5-76 Test Condition 76
Figure 5-78 Test Condition 78
Figure 5-80 Test Condition 80
Figure 5-82 Test Condition 82
Figure 5-84 Test Condition 84
Figure 5-86 Test Condition 86
Figure 5-88 Test Condition 88
Figure 5-90 Test Condition 90
Figure 5-92 Test Condition 92
Figure 5-94 Test Condition 94
Figure 5-96 Test Condition 96
Figure 5-98 Test Condition 98
Figure 5-100 Test Condition 100
Figure 5-102 Test Condition 102
Figure 5-104 Test Condition 104
Figure 5-106 Test Condition 106
Figure 5-108 Test Condition 108