SLVSAJ4E September 2010 – June 2026 TPS723-Q1
PRODUCTION DATA
The device has an internal current limit circuit that protects the regulator during transient high-load current faults or shorting events. The current limit is a brick-wall scheme. In a high-load current fault, the brick-wall scheme limits the output current to the current limit (ICL). ICL is listed in the Section 5.6 table. Also see, Figure 6-17 in the Section 6 section.
The output voltage is not regulated when the device is in current limit. When a current limit event occurs, the device begins to heat up because of the increase in power dissipation. When the device is in brick-wall current limit, the pass transistor dissipates power [(VIN – VOUT) × ICL]. If thermal shutdown is triggered, the device turns off. After the device cools down, the internal thermal shutdown circuit turns the device back on. If the output current fault condition continues, the device cycles between current limit and thermal shutdown. For more information on current limits, see the Know Your Limits application note.
Figure 7-5 shows a diagram of the current limit.
Figure 7-5 Current
LimitDo not drive the output less than 0.3V below the input. An output voltage less than 0.3V below the input voltage biases the body diode in the pass transistor, and allows current to flow from the input to the output. This current is not limited by the device. If this condition is expected, make sure to externally limit the reverse current. See the Reverse Current section for more details.