SLVSFT8F February 2023 – December 2023 TPS7H1111-SEP , TPS7H1111-SP
PRODUCTION DATA
The desired turn-on threshold is 1.8 V. This means that as the VIN rail is turned-on and begins rising, the TPS7H1111 will begin turning-on as soon as VIN reaches 1.8 V. While this is not enough headroom from VIN to VOUT for final regulation, the regulator will begin start-up and VIN will continue to its final voltage of 2.5 V. If desired, a higher voltage turn-on threshold could also be utilized (for example, 2.2 V).
By using Equation 3 and selecting an REN_TOP value 56.2 kΩ, the REN_BOT resistor can be calculated as shown in Equation 16.
A standard value 28 kΩ resistor is selected for REN_BOT. The worst case (highest) VIN(rising) threshold is calculated using Equation 3 and the max VEN(rising) threshold of 0.62 V. This is determined to be 1.86 V which is acceptable. The typical VIN(falling) is then calculated using Equation 4. This is determined to be 1.50 V which is also acceptable.
It is also important to ensure Equation 5 is followed to prevent possible SEFIs. As shown in Equation 17, VEN(final) = 0.83 V which is greater than the recommended 0.8 V.