SLVSGL6B July 2022 – October 2026 TPS1HC30-Q1
PRODUCTION DATA
The following figure shows the typical setup for a capacitive load application and the internal blocks that function when the device is used. Note that all capacitive loads have an associated "load" in parallel with the capacitor that is described as a resistive load but in reality it can be inductive or resistive.
The second key care about for this application is to make sure that the capacitive load can charge up completely without the device hitting thermal shutdown. The reason is because if the device hits thermal shutdown during the charging, the resistive nature of the load in parallel with the capacitor starts to discharge the capacitor over the duration the TPS1HC30-Q1 is off. Note that there are some application with high enough load impedance that the TPS1HC30-Q1 hitting thermal shutdown and trying again is acceptable; however, for most applications, the system must be designed so that the TPS1HC30-Q1 does not hit thermal shutdown while charging the capacitor.
With the current clamping feature of the TPS1HC30-Q1, capacitors can be charged up at a lower inrush current than other high current limit switches. This lower inrush current means that the capacitor takes a little longer to charge all the way up. The time that it takes to charge up follows the equation below.
However, because the VDS for a typical 3.3A application is much less than the VBB voltage (VDS ≅ 3.3A × 0.03Ω = 100mV, VBB ≅ 13.5V), the equation can be rewritten and approximated as
The following figure pictures charge timing.
Using this dt calculated based on the current limit, and finding the transient thermal impedance value at half the dt value, the junction temperature rise can be approximated by the Equation 5.
For more information about capacitive charging with high-side switches, see the How to Drive Resistive, Inductive, Capacitive, and Lighting Loads application note. This application note has information about the thermal modeling available along with quick ways to estimate if a high-side switch can charge a capacitor to a given voltage.