10 Revision History
Changes from Revision B (June 2024) to Revision C (April 2025)
- Added bullet "MagPack technology shields inductor and
IC"Go
- Deleted bullet "Measurements according to CISPR
available"Go
- Deleted "PSpice and SIMPLIS models available"
bulletGo
- Updated bullet with package options to include package height and
"with no bondwires" Go
- Deleted TPSM828303PVCBR (Advance information) from the Device
Information table. Go
- Deleted package height from the Device Information
tableGo
- Added TPSM828301 (VCB) and TPSM828302 (VCB) (Preview information) to
Device Information table Go
- Added "a family of 1A, 2A, and 3A, pin-to-pin compatible" in the
Description
Go
- Changed from "Based on the DCS-Control topology, the devices have a
fast transient response yet with small output capacitance" to "The devices use
DCS-Control topology for fast transient response with small output capacitance"
in the Description
Go
- Changed from "The power save mode prolongs battery life at low
output currents and the forced PWM mode maintains continuous conduction in the
inductor to reduce ripple at constant switching frequency" to "The power save
mode is for longer battery life and the forced PWM mode reduces ripple with
continuous conduction in the inductor at a quasi fixed switching frequency" in
the Description
Go
- Changed from "An internal soft-start circuit ramps the voltage up
tightly controlled and a power-good signal indicates correct output voltage" to
"An internal soft-start circuit reduces inrush current and a power-good signal
indicates correct output voltage" in the Description
Go
- Deleted "The devices support 100% mode" from the
Description
Go
- Changed from "3.0mm × 3.0mm × 1.95mm QFN package and 2.5mm × 2.6mm ×
1.95mm" to "3.0mm × 3.0mm QFN package and in the 2.5mm × 2.6mm" in the
Description
Go
- Deleted "Advance information (not Production Data)" table note from
TPSM828303PVCBR in the Device Options tableGo
- Added TPSM828303KPVCBR, TPSM828301APVCBR, and TPSM828302APVCBR with
"Preview information (not Production Data)" table note in the Device
Options table. Go
- Changed TPSM828303PVCBR advance information to TPSM828303APVCBR for
release to production in the Device Options table Go
- Added column with soft-start time information in the Device
Options tableGo
- Change the description of pin 8 in both Pin Functions tables
from "which is connected to the internal power MOSFET and the inductor. Avoid
connecting this pin to larger traces as this can increase EMI. this pin can stay
unconnected or be soldered " to "internally connected the inductor. For lowest
EMI, leave this pin unconnected or solder this pin "Go
- Deleted VOUT from line 1 in Absolute Maximum Ratings
Go
- Added two additional lines for voltage in Absolute Maximum
Ratings, one for pins SW (DC), VOS, and VOUT and one for SW (AC, <
10ns) with table note "While switching"Go
- Added parameter tSS in Electrical Characteristics table in
section STARTUP for device version TPSM828303xKGo
- Changed parameter name td(PG) to td(PGO) in section POWER GOOD for
deglitch delay during operationGo
- Added table note to parameter VFB in section REFERENCE VOLTAGE
indicating the parameter is a DC parameterGo
- Changed paragraph "The VCB package version uses MagPack technology for even
further EMI reduction. MagPack, a Texas Instruments proprietary integrated-magnetics
packaging technology, delivers the highest-performance power module design. Besides EMI
reduction, MagPack enhances efficiency and thermal properties of power modules. This
feature enables an industry-leading power density" to "The VCB package version uses
MagPack technology to deliver the highest-performance power module design. Leveraging the
Texas Instruments proprietary integrated-magnetics MagPack packaging technology, these
power modules deliver industry-leading power density, high efficiency and good thermal
performance, ease of use, and reduced EMI emissions"Go
- Added table note about inductance of the integrated
inductorGo
- Changed inductance of integrated inductor in the VCB package version
from 340nH to 400nH. Go
- Changed start-up time values from fixed values in text to references
into spec table. Go
- Added description about the relation between output capacitor
selection and start-up time with reference to the version TPSM82830xK for slower
start-upGo
- Added VOUT Accuracy sectionGo
- Changed PG signal delay time values from fixed values in text to references
into spec table. Go
- Changed inductance of VCB package version from 340nH to
400nH.Go
- Changed figure from fixed values for VIN and VOUT and the resistors
to references into the Design Parameters table and the BOM
tableGo
- Added resistor value for 1.8V VOUT in List of Components
tableGo
- Changed outdated instructions for using WEBENCH Tools to current
instructions Go
- Added three figures with the title "PG to VOUT
Influence"Go
- Changed outdated instructions for using WEBENCH Tools to current
instructions Go
Changes from Revision A (December 2023) to Revision B (June 2024)
- Added TPSM828303PVCBR (Advance Information)Go