SLVSH61D March 2025 – September 2026 TPS7H4102-SEP , TPS7H4104-SEP , TPS7H4104-SP
PRODUCTION DATA
The VIN pin provides power to internal control circuitry. The PVIN pins provide the input voltage (and power to the loads) to all the internal half-bridges (CH # 1 to CH # 4). Both pins have an input voltage range from 3V to 7V. The pins must be at the same nominal voltage and the pins must power-up and power-down at the same time. Generally this is achieved by providing the pins from the same voltage source (tied together).
Both VIN and PVIN have individual UVLO (under voltage lockout) rising thresholds, VUVLOR_VIN (2.7V typical) and VUVLOR_PVIN (2.44V typical), respectively. This is to make sure the device internal bias is sufficient for proper operation. Additionally, VIN and PVIN have individual UVLO falling thresholds, VUVLOF_VIN (2V typical) and VUVLOF_PVIN (2.52V typical), respectively. If the voltage falls and these values are reached, the device turns off. As PVIN and VIN are tied together in the application, the dominant UVLO for the device (or I.C.) is the VIN UVLO as is the higher threshold value during a rising and falling voltage.
If desired, the user can adjust the effective UVLO by using an external resistive voltage divider, connected between VIN and ENx. For more details, see Section 8.3.4.1.