SLVSH61D March 2025 – September 2026 TPS7H4102-SEP , TPS7H4104-SEP , TPS7H4104-SP
PRODUCTION DATA
In addition to the internal sequence up/down (using EN_SEQ), typical sequence-up methodologies as described below can be implemented using the SS_TRx, ENx, and PWRGDx pins.
The sequential method is shown in Figure 8-11. In this case channel # 1 and #2 of TPS7H4104 are used. As with any methodology discussed here, the figure can be expanded to any CHx (or from another point of load converter), however for simplicity the figure shows only 2 channels (in this case CH1 and CH2). The PWRGD1 pin of the first channel is coupled to the EN2 pin of the second channel, which enables the second power supply after the primary supply reaches regulation (typically 94% during a rising VOUTx voltage) . If a further delay is desired between sequencing of the first and second channel an optional CPWRGD1 capacitor can be included on PWRGD1 as well. This causes an RC delay based on the value of the power good pull-up resistor and the capacitor used.
Figure 8-12 shows the method implementing ratiometric sequencing by connecting the SS_TR1 and SS_TR2 pins of two channels together (in this case channels # 1 and 2). The regulator outputs (VOUT1 and VOUT2) ramp up and reach regulation at the same time.
Ratiometric and simultaneous power-supply sequencing can be implemented by connecting the resistor network of R1 and R2 (shown in Figure Ratiometric and Simultaneous Start-Up Sequence) to the output of the power supply that must be tracked or another voltage reference source. Using Equation 22 and Equation 23, calculate the tracking resistors to initiate the VOUT2 slightly before, after, or at the same time as VOUT1. Equation 24 is the voltage difference between VOUT1 and VOUT2.
To design a ratiometric start-up in which the VOUT2 voltage is slightly greater than the VOUT1 voltage when VOUT2 reaches regulation, use a negative number in Equation 22 and Equation 23 for ΔV. Equation 24 results in a positive number for applications where the VOUT2 is slightly lower than VOUT1 when VOUT2 regulation is achieved.
The ΔV variable is 0V for simultaneous sequencing. To minimize the effect of the inherent SS_TRx to VSNSx offset (SS_TRxSTART_UP = 22mV typical) in the soft-start circuit and the offset created by the pullup current source (ISS_TRx = 2.28μA typical) and tracking resistors, the SS_TRxSTART_UP and ISS_TRx are included as variables in the equations.
To provide proper operation of the device, the calculated R1 value from Equation 22 must be greater than the value calculated in Equation 25.