SLVSHK4 December 2025 MCT8376Z-Q1
PRODUCTION DATA
The device is fully protected for any cross conduction of MOSFETs. In half-bridge configuration, the operation of high-side and low-side MOSFETs are maintained to avoid any shoot-through currents by inserting a dead time (tdead). This is implemented by sensing the gate-source voltage (VGS) of the high-side and low-side MOSFETs and maintaining that VGS of high-side MOSFET has reached below turn-off levels before switching on the low-side MOSFET of same half-bridge as shown in Figure 7-14 and Figure 7-15.
Figure 7-14 Cross Conduction
Protection
Figure 7-15 Dead Time