SLVSHO1B March 2025 – October 2026 TPS1689
PRODUCTION DATA
PMBUS_ADDR is a manufacturer-specific command used for reading and configuring a user-specific device address apart from the addresses mentioned in Table 7-5. The device uses this address for I2C communication instead of the default value (0x40) when ADDR0 and ADDR1 pins are OPEN. This updated device address can be stored in the NVM and the device responds to this revised address upon power up next time.
This command uses the PMBus® read or write byte protocol.