SLVSHO1B March 2025 – October 2026 TPS1689
PRODUCTION DATA
CABLE_DROP is a manufacturer-specific command that allows configuring or reading an 8-bit reference threshold for the maximum cable voltage drop expected to implement the input cable fault detection feature. This command uses the PMBus® DIRECT format. When reading and writing to this register, use the coefficients shown in Table 7-65, Equation 14, and Equation 15.
This command uses the PMBus® read or write byte protocol.
Contents of this register are compared with the difference between PSU_VOLTAGE and VIN ADC telemetry values. If this difference value exceeds the value in the CABLE_DROP register, the VIN_CABLE_FAULT flags are set in the respective registers. The SMBA signal is asserted. When the difference between PSU_VOLTAGE and VIN ADC telemetry value falls below the CABLE_DROP threshold, and the CLEAR_FAULTS command is sent afterwards, this warning flag and alart clear. The details of this register are shown in Table 8-67.
| Bit | Name | Description | Minimum Value | Maximum Value | Default Value | Access |
|---|---|---|---|---|---|---|
7:0 | CABLE_DROP | Maximum cable voltage drop expected | 0x00h (0V) | 0xFFh (13.98V) | 0xFFh (13.98V) | Read/Write |
When the input cable fault is detected, the device:
sets the NONE_OF_THE_ABOVE/UNKNOWN bit in the STATUS_BYTE register
sets the NONE_OF_THE_ABOVE/UNKNOWN bit in the upper byte of the STATUS_WORD register
sets the VIN_CABLE_FLT bit in the STATUS_MFR_SPECIFIC_2 register
notifies the host asserting SMBA, if it is not masked setting the UNKNOWN bit low in the ALERT_MASK register
If this feature is not used, it is recommended to configure the setting to its maximum value to prevent unnecessary fault assertions.
A write command to this register must be preceded by the MFR_WRITE_PROTECT command to unlock the device first to prevent accidental or spurious writes.