SLVSHO1B March 2025 – October 2026 TPS1689
PRODUCTION DATA
READ_BB_RAM is a manufacturer-specific command used to read the contents of the Blackbox buffer RAM, which is seven (7) bytes deep as described in Section 7.3.14.11.
This command uses the PMBus® block read protocol with a block size of seven (7).
Table 8-67 presents details of the Blackbox RAM registers. There are seven (7) Blackbox RAM registers, starting from BB_RAM_0 to BB_RAM_6. Descriptions of all seven (7) registers (BB_RAM_0 to BB_RAM_6) are identical.
| Bit | Name | Value | Description | Default | Access |
|---|---|---|---|---|---|
7:5 | EVENT_ID | Event identifier | Read | ||
111 | VIN_UV_WARN | 000 | |||
110 | VIN_OV_WARN | ||||
101 | OC_WARN | ||||
100 | OT_WARN | ||||
011 | OC_DET | ||||
010 | VOUT_UV_WARN | ||||
001 | IN_OP_WARN | ||||
000 | None | ||||
4 | BB_TMR_EXP | Blackbox timer expiry | |||
1 | Blackbox timer overflowed at least once since the last event | 0 | |||
0 | Blackbox timer has not overflowed | ||||
3:0 | BB_TICK | 0000 | Blackbox tick timer | 0000 |
The Blackbox RAM contents get reset under the following events:
Input power recycle at VIN or VDD pin
ENABLE recycling
CLEAR_FAULTS command
Initiation of an auto-retry sequence