SLVSHO1B March 2025 – October 2026 TPS1689
PRODUCTION DATA
OPERATION is a PMBus® standard command that controls the FET inside the eFuse in conjunction with the input from the EN/UVLO pin. This command may be used to switch the eFuse ON and OFF under host control. It is also used to re-enable the eFuse after a fault-triggered shutdown.
This command uses the PMBus® read or write byte protocol.
| Bit | Name | Value | Description | Default | Access |
|---|---|---|---|---|---|
7 | ON | Enable | Read/Write | ||
1 | eFuse output enabled | 1 | |||
0 | eFuse output disabled | ||||
6:0 | RESERVED | 0000000 | N/A | 0000000 |
This command should be preceded by the Section 7.3.14.7.1.10 command to unlock the device first to prevent accidental/spurious writes. If the WP# pin is pulled low, the write access is completely disabled in hardware and MFR_WRITE_PROTECT command has no effect.
Writing an OFF command followed by an ON command will clear all the fault and warning bits in the status registers. Writing only an ON command after a fault-triggered shutdown will not clear the status registers.
OFF command engages quick output discharge (QOD).