SLVSHO1B March 2025 – October 2026 TPS1689
PRODUCTION DATA
RESTORE_FACTORY_DEFAULTS is a standard PMBus® command that initializes or resets all the configuration RAM registers to the hardware defaults. Read the INIT_DONE bit in the STATUS_MFR_SPECIFIC_2 register to check if initialization is completed successfully.
This command uses the PMBus® send byte protocol. There is no data byte for this command. This command is write only.
This command must be preceded by the Section 7.3.14.7.1.10 command to unlock the device first to prevent accidental/spurious writes. If the WP# pin is pulled low, the write access is completely disabled in hardware and Section 7.3.14.7.1.10 command has no effect.