SLVSHS0C March 2025 – September 2026 TPS482H85-Q1
PRODUCTION DATA
In the OFF state, when DIAG_EN is high, there is an internal pull-up resistor RPU that pulls up a channel to VBB. The specific channel that gets pulled up is based on the selection of SEL, and the other channels do not have the pull-up resistor engaged.
If there is load present at the selected channel, then the output voltage is pulled to around 0V, as the load is much stronger than the RPU. In the case of an open load, the output voltage pulls close to the supply voltage by the RPU. If VBB - VOUT < VOL,off for the selected channel, the FLT pin goes low to indicate the fault to the MCU, and the SNS pin is pulled up to ISNSFH.