SLVSHS0C March 2025 – September 2026 TPS482H85-Q1
PRODUCTION DATA
The ACTIVE state is when any of the channel outputs are on by the ENx pin associated. In the ACTIVE state, the external resistor on the ILIM pin sets the current limit value. If the DIAG_EN pin is pulled high while in the ACTIVE state, the SNS pin outputs a proportional current to the load current of the channel associated to the SEL pins configuration until a fault occurs on that channel. The device can transition out of the ACTIVE state by turning off all of the channels while DIAG_EN is high or low, or a fault occurring. If all of the channels turn off and DIAG_EN is high, the device transitions into the DIAGNOSTIC state. If all of the channels turn off and the DIAG_EN pin is low, then the device transfers into the STANDBY DELAY state. However, if the ENx pins are still high and a fault occurs, the device transitions into the FAULT state.