SLVSII7 December 2025 TPSM8D7420 , TPSM8D7620
PRODUCTION DATA
The adjustable switching frequency is set using a resistor from the RT pin to AGND. See Table 7-4 below for example resistor values. A resistor value that falls outside of the recommended range can cause the device to stop switching. Do not apply a pulsed signal to this pin to force synchronization. If synchronization is needed, use the SYNC pin.
The TPSM8D7x20 has two total switching channels. The switching frequency of both channels is set by the RT pin. All channels on this module are required share the same switching frequency in steady-state to verify that each channel has the correct phase.
For example, for fSW = 400kHz, RT = (15.92 / 0.4) - 0.526 = 39.27, so a 39.2kΩ resistor is selected as the closest choice.
| RT (kΩ) | CALCULATED FREQUENCY (kHz) |
|---|---|
| 6.81 | 2170 |
| 10.0 | 1512 |
| 15.4 | 1000 |
| 19.6 | 791 |
| 23.7 | 657 |
| 31.6 | 496 |
| 39.2 | 402 |