SLVSIN9 June 2026 LM25192-Q1
PRODUCTION DATA
In the voltage control loop, the LM25192-Q1 has a high-gain transconductance amplifier that generates an error current proportional to the difference between the internal feedback voltage and a programmable precision reference, VREF. The transconductance of the amplifier is 1000µS. The voltage loop error amplifier takes the control when the internal minimum function block, IMIN SELECTOR, selects the current from the voltage loop error amplifier as shown in the following figure.
The voltage control loop requires an external compensation network. TI generally recommends a type-II compensation network for peak current-mode control.