SLVSJY3A August 2026 – October 2026 BQ25350
PRODUCTION DATA
The BATFET functions as a load switch between battery and system when the converter is not running. By changing the state of BATFET from on to off, systems connected to SYS can be power cycled. A system reset also resets all registers to POR state. Any of the following conditions will initiate a system power reset:
When BATFET_CTRL_WVBUS is set to 1, system power reset will proceed if SYS_RESET = 1, regardless of whether or not VBUS is present. There is a delay of tBATFET_DLY before initiating the system power reset.
The system power reset can be initiated from the battery only condition or from the forward charging mode with adapter present.