SLVSM93 October 2026 TMUX4051-EP
ADVANCE INFORMATION
| PIN | TYPE(1) | DESCRIPTION(2) | |
|---|---|---|---|
| NAME | NO. | ||
| S4 | 1 | I/O | Source pin 4. Signal path can be an input or output. |
| S6 | 2 | I/O | Source pin 6. Signal path can be an input or output. |
| D | 3 | I/O | Drain pin (common). Signal path can be an input or output. |
| S7 | 4 | I/O | Source pin 7. Signal path can be an input or output. |
| S5 | 5 | I/O | Source pin 5. Signal path can be an input or output. |
| EN | 6 | I | Active low logic enable. When this pin is high, all switches are turned off. Section 10 lists how the A[2:0] address inputs determine which switch is turned on when this pin is low. |
| VSS | 7 | P | Negative power supply. This pin is the most negative power-supply potential. For reliable operation, connect a decoupling capacitor ranging from 0.1µF to 10µF between VSS and GND. |
| GND | 8 | P | Ground (0V) reference |
| A2 | 9 | I | Address line 2. Section 10 provides information about how A2 controls the switch configuration. |
| A1 | 10 | I | Address line 1. Section 10 provides information about how A1 controls the switch configuration. |
| A0 | 11 | I | Address line 0. Section 10 provides information about how A0 controls the switch configuration. |
| S3 | 12 | I/O | Source pin 3. Signal path can be an input or output. |
| S0 | 13 | I/O | Source pin 0. Signal path can be an input or output. |
| S1 | 14 | I/O | Source pin 1. Signal path can be an input or output. |
| S2 | 15 | I/O | Source pin 2. Signal path can be an input or output. |
| VDD | 16 | P | Positive power supply. This pin is the most positive power-supply potential. For reliable operation, connect a decoupling capacitor ranging from 0.1µF to 10µF between VDD and GND. |
Figure 4-2 TMUX4052-EP DYY Package, 16-Pin SOT-23-THIN (Top View)| PIN | TYPE(1) | DESCRIPTION(2) | |
|---|---|---|---|
| NAME | NO. | ||
| S0B | 1 | I/O | Source pin 0 of mux B. Signal path can be an input or output |
| S2B | 2 | I/O | Source pin 2 of mux B. Signal path can be an input or output. |
| DB | 3 | I/O | Drain pin (common) of mux B. Signal path can be an input or output. |
| S3B | 4 | I/O | Source pin 3 of mux B. Signal path can be an input or output. |
| S1B | 5 | I/O | Source pin 1 of mux B. Signal path can be an input or output. |
| EN | 6 | I | Active low logic enable. When this pin is high, all switches are turned off. Section 10 lists how the A[2:0] address inputs determine which switch is turned on when this pin is low. |
| VSS | 7 | P | Negative power supply. This pin is the most negative power-supply potential. For reliable operation, connect a decoupling capacitor ranging from 0.1µF to 10µF between VSS and GND. |
| GND | 8 | P | Ground (0V) reference |
| A1 | 9 | I | Address line 1. Section 10 provides information about how A1 controls the switch configuration. |
| A0 | 10 | I | Address line 0. Section 10 provides information about how A0 controls the switch configuration. |
| S3A | 11 | I | Source pin 3 of mux A. Signal path can be an input or output. |
| S0A | 12 | I/O | Source pin 0 of mux A. Signal path can be an input or output. |
| DA | 13 | I/O | Drain pin (common) of mux A. Signal path can be an input or output. |
| S1A | 14 | I/O | Source pin 1 of mux A. Signal path can be an input or output. |
| S2A | 15 | I/O | Source pin 2 of mux A. Signal path can be an input or output. |
| VDD | 16 | P | Positive power supply. This pin is the most positive power-supply potential. For reliable operation, connect a decoupling capacitor ranging from 0.1µF to 10µF between VDD and GND. |
Figure 4-3 TMUX4053-EP DYY Package,
16-Pin SOT-23-THIN (Top View)| PIN | TYPE(1) | DESCRIPTION(2) | |
|---|---|---|---|
| NAME | NO. | ||
| S2B | 1 | I/O | Source pin B of switch 2. Signal path can be an input or output. |
| S2A | 2 | I/O | Source pin A of switch 2. Signal path can be an input or output. |
| S3B | 3 | I/O | Source pin B of switch 3. Signal path can be an input or output. |
| D3 | 4 | I/O | Drain pin (common) of switch 3. Signal path can be an input or output. |
| S3A | 5 | I/O | Source pin A of switch 3. Signal path can be an input or output. |
| EN | 6 | I | Active low logic enable. When this pin is high, all switches are turned off. Section 10 lists how the A[2:0] address inputs determine which switch is turned on when this pin is low. |
| VSS | 7 | P | Negative power supply. This pin is the most negative power-supply potential. For reliable operation, connect a decoupling capacitor ranging from 0.1µF to 10µF between VSS and GND. |
| GND | 8 | P | Ground (0V) reference |
| SEL3 | 9 | I | Logic control select pin 3. Section 10 provides controls switch 3 configuration |
| SEL2 | 10 | I | Logic control select pin 2.Section 10 provides controls switch 2 configuration |
| SEL1 | 11 | I | Logic control select pin 1.Section 10 provides controls switch 1 configuration |
| S1A | 12 | I/O | Source pin A of switch 1. Signal path can be an input or output. |
| S1B | 13 | I/O | Source pin B of switch 1. Signal path can be an input or output. |
| D1 | 14 | I/O | Drain pin (common) of switch 1. Signal path can be an input or output. |
| D2 | 15 | I/O | Drain pin (common) of switch 2. Signal path can be an input or output. |
| VDD | 16 | P | Positive power supply. This pin is the most positive power-supply potential. For reliable operation, connect a decoupling capacitor ranging from 0.1µF to 10µF between VDD and GND. |