SLVUBX1 December 2020 TPS63810
The BOOSTXL-TECDRV BoosterPack is an evaluation platform designated to highlight the TPS63810 use as a driver for a thermoelectric cooling (TEC) module.
The BOOSTXL-TECDRV interfaces to LaunchPad development platforms using the XL connector format. To use the BOOSTXL-TECDRV BoosterPack GUI a specific LaunchPad (the MSP-EXP432P401R) must be used. The LaunchPad communicates to the TPS63810 through its I2C interface and also acts as a USB-to-PC GUI communication bridge.
The BOOSTXL-TECDRV requires a LaunchPad or external master controller to evaluate the TPS63810.
The MSP-EXP432P401R LaunchPad is controlled by commands received from the BOOSTXL-TECDRV BoosterPack GUI. The LaunchPad sends data to the GUI for display. If a LaunchPad is not used, the BoosterPack plug-in module format allows an alternate external host to communicate with the TPS63810 using the LaunchPad connectors.
The BOOSTXL-TECDRV incorporates circuitry and components with the following features:
The BOOSTXL-TECDRV requires an external 3.3-V power supply to power the TPS63810.
Figure 1-1shows the BOOSTXL-TECDRV architecture along with the key components and blocks listed in the features.
Figure 1-1 BOOSTXL-TECDRV Block Diagram