SLVUBX1 December   2020 TPS63810

 

  1.   Trademarks
  2. 1Introduction
  3. 2Quick Start
    1. 2.1 Step 1: Software Installation
    2. 2.2 Step 2: Firmware Completition and Flashing
    3. 2.3 Step 3: Hardware Setup
    4. 2.4 Step 4: GUI
  4. 3System Overview
  5. 4Hardware Overview
    1. 4.1 Buck-Boost Converter
    2. 4.2 Thermoelectric Cooler (TEC)
    3. 4.3 LaunchPad
    4. 4.4 Voltage Reference
    5. 4.5 Temperature Sensor
  6. 5Firmware Overview
  7. 6Graphical User Interface (GUI)
  8. 7Setup Details
  9. 8Bill of Materials, PCB Layout, and Schematic
    1. 8.1 Bill of Materials
    2. 8.2 PCB Layout
    3. 8.3 Schematic

Step 2: Firmware Completition and Flashing

Depending on the used temperature sensor and the TEC module, the LaunchPad firmware needs to be completed. This can be done using the Energia IDE or the cloud version of the CCS IDE. The completed firmware then needs to be downloaded to the LaunchPad using the micro USB cable provided with the LaunchPad kit. Details regarding these steps can be found in Section 7.