SLVUBZ4 February 2021 TPS25750
After the form has been sufficiently filled out, the option to Generate Full Flash Binary will enable on the right side panel, outlined in black in Figure 2-8. By clicking the button, a binary file will be downloaded. The binary file can then be used to flash the hardware device. The default file name for the downloaded binary file is fullFlash.bin.