SLVUBZ4 February 2021 TPS25750
The required software is available at the TI Gallery, and can be run from the web browser, provided that Chrome, Firefox, or Safari is used. If this is desired, TI Cloud Agent needs to be installed as a browser extension as well as on the PC. When the application is launched, instructions will appear for installing TI Cloud Agent.
The software may also be run natively on the PC. If this is desired, GUI Composer Runtime needs to be installed natively. To install GUI Composer Runtime, click on the downwards-facing arrow inside one of the applications listed in the Gallery, and look towards the bottom set of links that appear. After selecting your native operating system, open the installer and follow the prompts to install the program.