SLVUC46E March   2021  – November 2024

PRODUCTION DATA  

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Overview
      1. 1.1.1 Purpose and Scope
      2. 1.1.2 Supported EVMs
  5. 2Evaluation Hardware Overview
    1. 2.1 Connections Overview
    2. 2.2 Connection Details
      1. 2.2.1 Common Connectors and Headers Across all EVM Variants
      2. 2.2.2 MCU Reset and User Button
      3. 2.2.3 Communication Interfaces
      4. 2.2.4 Supply Input
      5. 2.2.5 Current Limit Header (RIPROPI)
      6. 2.2.6 Device Signal and Control Header
      7. 2.2.7 Device Signal Test Points
    3. 2.3 LED Indicators
    4. 2.4 Headers and Connectors (Hardware Device Variant)
    5. 2.5 Headers and Connectors (SPI variant)
  6. 3EVM GUI Control Application
    1. 3.1 MSP430 FET Drivers
    2. 3.2 Cloud-based GUI
    3. 3.3 Local Installation
  7. 4EVM GUI Operation
    1. 4.1 Hardware Setup
    2. 4.2 Launching the DRV824x_DRV814x_DRV8x63-Q1EVM GUI Application
    3. 4.3 Using the DRV824x_DRV814x_DRV8x63-Q1EVM GUI Application
      1. 4.3.1 Register Map Page (SPI Device Variant)
      2. 4.3.2 Driver Control Page (SPI Device Variant)
      3. 4.3.3 Driver Control Page (HW Device Variant)
      4. 4.3.4 Updating Firmware
  8. 5Revision History

Local Installation

Follow these instructions for downloading and installing the latest version of the EVM GUI application:

  1. The EVM GUI application installer can also be downloaded from the TI GUI Composer Gallery.
  2. From the gallery, click the DRV8243S-Q1EVM, DRV8243H-Q1EVM, DRV8244S-Q1EVM, DRV8244H-Q1EVM, DRV8245S-Q1EVM icon in the latest version and select the installer for your operating system (Windows, Linux or Mac). Refer back to in the previous section for a visual depiction of the Gallery page.
  3. Decompress the .zip file.
  4. From the decompressed archive, run the installer: for example, “DRV824x_DRV814x_DRV8x63-Q1EVM-GUI-1.2.0.setup-win" (refer to Figure 3-4). If the GUI Composer Runtime has not been installed, then the installer takes care of this. The installer contents looks slightly different for each OS, but is self-explanatory.
    DRV8243S-Q1EVM, DRV8243H-Q1EVM, DRV8244S-Q1EVM, DRV8244H-Q1EVM, DRV8245S-Q1EVM GUI Application Archive ContentsFigure 3-4 GUI Application Archive Contents
  5. The GUI application is now ready to run on the local machine after completing the hardware setup in the next section.