Follow the instructions to perform the power-up into short test:
- Confirm that the experiment is setup initially as per the instructions in Section 3.1.
- Disconnect the electronic load at the output of eFuse.
- Set the input supply voltage VIN to 12V and current limit to 30A. Keep the power supply OFF.
- Connect the negative terminal of power supply to J3-1 and positive terminal of power supply to J3-2
- Short the output of the EVM to ground. For example, short VOUT1 (connector
J2-1) to PGND (connector J2-2) through a cable.
- Turn ON the power supply.