Use the following instructions to perform the input hot-plug test on the LM7320 eFuse:
- Confirm that the experiment is setup initially as per the
instructions in Section 3.1.
- Configure the jumper J5 position to the desired start-up slew
rate as detailed in Table 2-3.
- Connect the negative terminal of the power supply to connector
J3-1.
- Set the input supply voltage VIN to 12V and current limit to
10A.
- Connect the positive terminal of the power supply to connector
J3-2. Enable the power supply.
- Disconnect the electronic load at the output.
- Throughout the test, use an oscilloscope to observe the
waveforms at IMON(TP10), VIN(TP2), VOUT(TP1) and input current.