The section provides procedure for the
EVM software installation. The DAC90802EVM software is portable; there is
no GUI installation required other than installing the FPGA controller (Opal Kelly
XEM7310A75) front panel driver. The EVM software is compatible with the Windows® 11
operating system. Before installing the software, verify that the DAC90802EVM is not connected to the
local machine. Follow the steps to install the driver, unzip the GUI to a folder of
your choice, and prepare the GUI for use:
- Download the Opal Kelly front
panel driver from https://pins.opalkelly.com/downloads as shown in Figure 3-1.
- Install the Opal Kelly front
panel driver by double-clicking on FrontPanelUSB-DriverOnly-5.3.6.exe.
- Follow the on-screen instructions
to complete the Opal Kelly front panel driver installation as shown in Figure 3-2.
- Download the latest version of
the EVM GUI software from the order and start development subsection of the DAC90802EVM tool folder on ti.com.
- Extract the downloaded zip file
to a desired location on your local machine.
- After extracting the downloaded
zip file, the folder contains the DAC90802EVM
GUI.exe application and an internal folder containing the GUI dependencies.
- Keep the internal folder in the
same location as the executable file. For proper GUI operation, do not move or
delete the internal folder.