SLWU067D November 2009 – March 2022
Selection of various modes of operation of the ADS41xx/58B18EVM is most often controlled by jumpers on the EVM, either by placing shunts on 0.025-inch square jumper posts or by installation of surface mount 0-Ω resistors. In general, the use of 0-Ω resistors as jumpers are used in the clock or signal path where signal integrity is critical and jumper posts are used for static or low-speed control paths. Figure 2-1 shows the relative location of the jumpers, connectors, and switches used on the ADS41xx/58B18EVM. Figure 2-2 shows the relative locations of most of the resistors and surface-mount 0-Ω jumper locations used on the EVM. In the description of the circuit options in the following sections, each operational mode is accompanied by a table entry that details the jumper or resistor changes that enable that option. Figure 2-1 and Figure 2-2 can assist the user to quickly identify where these jumpers are located on the EVM.
Figure 2-1 ADS41xx Jumpers
Figure 2-2 ADS41xx/58B18 Surface JumpersThe following sections describe the function of individual circuits. See the relevant data sheet for device operating characteristics.