SLWU087E november 2013 – june 2023
This section describes the operation when testing with a DAC5688 EVM that has a CMOS input interface.
J1 pin 1 of the TSW1400 connector plugs into J2 pin 1 on the DAC5688 EVM
Figure 5-5 TSW1400EVM Interfacing to the CMOS Connectors of a DAC5688EVMUsing the DAC5688 EVM GUI, load the EVM with the test file called “example”. This can be found at C:\Program Files (x86)\Texas Instruments\DAC5688\DAC5688 Configuration Files. This sets up the DAC5688 to receive a WCDMA test pattern from the TSW1400 with a data rate of 122.88 MHz. CLK2 of DAC5688 operates at 491.52 MHz and the DAC interpolation is set to 4x, requiring the input data rate to be at 122.88 MHz.
In the DAC5688 GUI, go to the CDCM7005 tab and set the Y3 Output (OUTCLK3) to divide by 4, LVCMOS, and inverting per Figure 5-6.
Figure 5-6 CDCM7005 Tab on DAC5688 GUIThis generates an inverted 122.88-MHz clock used by the TSW1400 to generate the CMOS test pattern.
The CMOS data rate for the TSW1400 EVM should never exceed 250 MHz. This rate is set by the CMOS_CLOCK input provide to J7. When operating at frequencies near this limit, the user may need to adjust the delay of this signal to meet the timing specs of the DAC under test.
On the DAC5688 EVM, there is an option to use a spare output of the CDCM7005 clock generator as a clock source. In this example, the OUTCLK3 of the CDCM7005 is inverted for optimized setup and hold time. Another way to adjust the delay is to use different cable lengths for this clock source.
If opening the HSDC Pro GUI for the first time, when setting up for pattern generator mode, make sure “DAC” in the top right side of the GUI is selected. This targets the EVM for this test example. In the “Select DAC” button of the GUI, click on the drop down arrow and select “cmos”. This firmware is used by most High Speed CMOS DAC EVM’s.
Click on “Yes” when asked “Do you want to update the firmware for DAC”. The firmware setup is loaded during this process, which takes approximately 20 seconds. After the firmware load has completed, the LED’s labeled USER_LED (0–7) will now turn on except for USER_LED 5. USER_LED 3 is used to indicate the status of a second PLL, and USER_LED 5 indicates if there is a FIFO overflow (error) of the transmit data.
If the TSW1400 is not receiving a valid clock from the DAC EVM, USER_LED3 and USER_LED4 are off.
For this test, at the top of the GUI, set the following parameters:
The display panel of the GUI is updated, showing the test data that is transmitted to the DAC EVM in both codes and frequency domain as shown in Figure 5-7.
Figure 5-7 GUI After Test File LoadedIf the DAC5688 EVM is configured for IF output, connect a spectrum analyzer to either SMA J4 (IOUTB2) or J9 (IOUTA2) of the EVM. The DAC example file has a NCO setting of 61.44 MHz and the test pattern IF is centered at 30 MHz. The signal should be a single carrier centered around 91.44 MHz, as shown in Figure 5-8.
The DAC5688 EVM has the default setup as RF output. The modulator output location will be at the LO frequency plus 91.44 MHz. For details about IF and RF output configuration settings, see section 4.7 of the DAC5688 EVM User’s Guide (SLAU241).
Figure 5-8 DAC5688 IF Output