SLWU087E november 2013 – june 2023
The Channel Power option, when selected, will display the calculated power of the channels selected in the parameter column on the left side of the GUI. This option will have three new setting windows displayed in the bottom left of the GUI for the user to select the number of channels (up to 5), the signal width, and channel separation of the captured data to be used for channel power measurements. Each channel that is selected for a power measurement will have two cursors, one labeled CxL and the other CxU. The "x" value will indicate the actual channel number. Figure 3-37 shows an example of a 3 channel power measurement while using the simulated ADC input function. The input test pattern is called "WCDMA_TM1_complexIF30MHZ_Fdata245.76MHZ_1000.tsw", which is located in the test files directory.
Figure 3-37 Three Channel Power Measurement Example