SLWU087E november   2013  – june 2023

 

  1.   1
  2.   High Speed Data Converter Pro GUI
  3.   Trademarks
  4. 1 Introduction
  5. 2 Software Start up
    1. 2.1 Installation Instructions
    2. 2.2 USB Interface and Drivers
    3. 2.3 Device ini Files
  6. 3 User Interface
    1. 3.1 Toolbar
      1. 3.1.1 File Options
        1. 3.1.1.1 User Profiles
        2. 3.1.1.2 Resize Window
      2. 3.1.2 Instrument Options
        1. 3.1.2.1 TSW14J56 and High Speed Data Converter (HSDC) Pro Eye Quality Analysis
        2. 3.1.2.2 IO Delay
        3. 3.1.2.3 JESD204B Error Injection
        4. 3.1.2.4 FPGA Registers Write Read
      3. 3.1.3 Data Capture Option
        1. 3.1.3.1 Capture Option
        2. 3.1.3.2 Trigger Option
        3. 3.1.3.3 Using Multiple TSW14xxx and ADC EVM’s for Simultaneous Capture using Trigger Option
          1. 3.1.3.3.1 Hardware Setup
          2. 3.1.3.3.2 Setting up the Slave Board
          3. 3.1.3.3.3 Setting up the Master Board
          4. 3.1.3.3.4 Read Captured Memory from the Slave Board
      4. 3.1.4 Test Options
        1. 3.1.4.1  Notch Frequency Bins
        2. 3.1.4.2  2 Channel Display and Cursor Lock
        3. 3.1.4.3  Analysis Window Markers
        4. 3.1.4.4  X-Scale in Time
        5. 3.1.4.5  Y-Scale in Voltage
        6. 3.1.4.6  Other Frequency Options
        7. 3.1.4.7  NSD Marker
        8. 3.1.4.8  Phase Plot
        9. 3.1.4.9  Phase in Degree
        10. 3.1.4.10 Histogram
        11. 3.1.4.11 Disable User Popups
        12. 3.1.4.12 HSDC Pro Lite Version
      5. 3.1.5 Help
    2. 3.2 Status Windows
    3. 3.3 Mode Selection
    4. 3.4 Device Selection
    5. 3.5 Skip Configuration
    6. 3.6 Capture Button (ADC Mode Only)
    7. 3.7 Test Selection (ADC Mode only)
      1. 3.7.1 Single Tone FFT
        1. 3.7.1.1 Parameter Controls
        2. 3.7.1.2 ADC Captured Data Display Pane
        3. 3.7.1.3 FFT Power Spectrum
        4. 3.7.1.4 Overlay Unwrap Waveform
        5. 3.7.1.5 Single Tone FFT Statistics
      2. 3.7.2 Multi Channel Display
      3. 3.7.3 Unit Selection
      4. 3.7.4 Time Domain
      5. 3.7.5 Two Tone
      6. 3.7.6 Channel Power
    8. 3.8 DAC Display Panel (DAC Mode only)
      1. 3.8.1 Send Button (DAC Mode Only)
      2. 3.8.2 Load File to Transfer into TSW14xxx Button
      3. 3.8.3 Parameter Controls
    9. 3.9 I/Q Multi-Tone Generator
  7. 4 ADC Data Capture Software Operation
    1. 4.1 Testing a TSW1400 EVM with an ADS5281 EVM
    2. 4.2 Testing a TSW1400EVM with an ADS62P49EVM (CMOS Interface)
  8. 5 TSW1400 Pattern Generator Operation
    1. 5.1 Testing a TSW1400 EVM with a DAC3152 EVM
    2. 5.2 Loading DAC Firmware
    3. 5.3 Configuring TSW1400 for Pattern Generation
    4. 5.4 Testing a TSW1400 EVM with a DAC5688EVM (CMOS Interface)
  9. 6 TSW14J58 Functional Description
    1. 6.1 Testing the TSW14J58 EVM with an ADC12DJ3200 EVM
  10. 7 TSW14J57 Functional Description
    1. 7.1 Testing the TSW14J57 EVM with an ADC34J45 EVM
  11. 8 TSW14J56 Functional Description
    1. 8.1 Testing the TSW14J56 EVM with an ADC34J45 EVM
  12. 9 TSW14J50 Functional Description
    1. 9.1 Device Selection
  13. 10TSW14J10 Functional Description
    1. 10.1 DAC and ADC GUI Configuration File Changes When Using a Xilinx Development Platform
    2. 10.2 DAC38J84EVM GUI Setup Example
  14.   A Signal Processing in High Speed Data Converter Pro
    1.     A.1 Introduction
    2.     A.2 FFT Calculation from Time Domain Data
      1.      A.2.1 FFT Window Correction Factor
    3.     A.3 FFT Filtering
    4.     A.4 Single Tone Parameters
      1.      A.4.1 Number of Neighboring Bins for each FFT Window
    5.     A.5 Fundamental Power
      1.      A.5.1 Harmonic Distortions
      2.      A.5.2 SNR
      3.      A.5.3 SFDR
      4.      A.5.4 THD
      5.      A.5.5 SINAD
      6.      A.5.6 ENOB
      7.      A.5.7 Next Spur
    6.     A.6 Two Tone Parameters
    7.     A.7 Average FFT Calculation
    8.     A.8 NSD Calculation
  15.   B History Notes
  16.   C Revision History

Time Domain

The Time Domain option, when selected, displays the ADC captured data as digital codes in the time domain. The statistics of the codes reported on the left side of the GUI are minimum value (Min), maximum value (Max), Standard deviation (St. Dev), Mean, Median, RMS, Peak-to-Peak and PAR.

M1, M2, Delta – Displays the code value of the location of markers M1 and M2. These markers can be moved around on the display with the mouse. The Delta parameter displays the code value difference between M2 and M1.

The position of the markers M1 and M2 are editable in the above table. For example, to set a position for Marker M1, just click on the Units column of M1 row cell, and enter the required value to see the change in M1 Marker Position.

Furthermore, the time domain RMS value is calculated with the DC power of the signal. The Standard deviation value does not include the DC power.

The following steps explain how the HSDC Pro calculates the RMS and Standard Deviation values.

  1. Standard Deviation: Square root of (Sum of (square of(All elements of the Time Domain Channel data array - Mean))/(Time Domain Channel data array size - 1))

    The VI calculates the standard deviation value using Equation 5.

    Equation 5. GUID-FFC12B73-4093-42D9-A9D7-19B37E1CA549-low.gif

    where Ψx is the standard deviation value and n is the number of elements in X and the mean value is represented by µ.

  2. RMS: Square root of (Sum of (square of(All elements of the Time Domain Channel data array))/(Time Domain Channel data array size - 1))

    The VI calculates rms value using Equation 6.

    Equation 6. GUID-DE2F49BF-CD6C-46A6-AFE7-006C8FB1CBCE-low.gif

    where Ψx is rms value and n is the number of elements in X.